Hi
In the current design of line driver based on the LM158QML I need to provide its output tolerate to +/- 16.5 fault voltage from receiver both in ON and in OFF state. For this was used the next solution:
But at worth case simulation I see that the voltage of OpAmp's output is very low.
If I really need these protection diodes (D7, D8)? Vcc=6Vdc and at simulation Vcc=0V.
The simulation was performed without diodes.
Best regards. Ilya