Hi Ti experts,
I have some questions regarding TPS50601-SP. Would you please kindly help to clarify? Thank very much.
1. On TPS50601-SP data sheet page9 (electrical characteristics) - What’s the meaning of “minimum off time” and test condition? If minimum off time is 500ns, does it mean the duty cycle must be smaller than 50% at 1MHz (max on time = period –min off time = 1us-500ns=500ns)?
2. On TPS50601-SP data sheet Page13 (Typical characteristics) -
What’s the difference between minimum controllable on-time and duty ratio?
For example, as in fig15, the minimum controllable on-time at 25degree is 100ns, so the minimum controllable duty ratio should be (assume frequency is 500kHz): 100ns/2us = 5%. But in fig 16 it is higher than 5%.
Why there is this difference?
Best regards,
Peter