Do we have any information on the output noise of the DAC121S101QML-SP? Is see the error specifications, but nothing regarding the noise. Do we have anything on this?
Thanks for your help with this!
Richard Elmquist
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Do we have any information on the output noise of the DAC121S101QML-SP? Is see the error specifications, but nothing regarding the noise. Do we have anything on this?
Thanks for your help with this!
Richard Elmquist
Hello Richard,
Here are the noise results from simulation:
Conditions: VDD=5V, 25 degrees C, typ process, code=2048 (midpoint=worst case for R string)
Spot Noise (volts squared)
@ 1Hz 1.87e-12
@10Hz 2.88E-13
@100Hz 4.5e-14
@1kHz 7.3e-15
Integrated Noise (volts squared)
1 Hz – 100 MHz 1.47E-8
Kirby,
Thanks so much for your fast response!
I will let you know if the customer has any further questions.
Richard Elmquist