Other Parts Discussed in Thread: THS4521, ADS1278
Hi,
I am using ADS1278-EP in conjuction with SM470R1B1M in my data acquisition system. The readings were quite unstable while i have stable voltage at ADC inputs. I am using channels 1,2 and 3. I have a voltage around 3mV , 260 mV, 2.4V respectively. Readings are stable only at channel 3. when i have low input voltage the readings are quite unstable.
I always read +/- 3mV mean at 260mV and quite unstable at 3mV range.
The readings are from a transducer, we connected through THS4521 Diff op-amp and without op-Amp each case it is same.
ADS1278 is operating low speed mode. CLOCK is = 3.75 MHz and SPICLK = 1.875MHz.
Any help appreciated.
Regards,
Pavan.