Hi everybody!
I'm using a UC1707-SP Dual-Channel Power Driver (part number 5962-8761901V2A) for a high-reliability, spaceborne system.
In my application, it's driven by a microcontroller, with two 0÷3.3V PWM signals, and drives two power MOS.
The PWM signals are isolated: they go through 1:1 transformers which are placed between the microcontroller and the MOS driver.
The problem is the loss of the DC components of PWM signals due to transformers. The PWM signals at UC1707-SP inputs have -1.65÷+1.65V levels.
I tested the UC1707-SP in this condition and it seems to work properly, despite the fact that the required "Digital input high level" is 2.2V (by datasheet).
Do you think that this configuration is "doable" (after more extensive tests to prove it works) or that it's unacceptable?
Thanks in advance,
EF