This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC1846-DIE: UC1846

Part Number: UC1846-DIE
Other Parts Discussed in Thread: UC1846

hi.

i am using UC1846 for a DC-DC Converter application,

Where RT pin of the ic is fixed to 11.2kohm and capacitor to CT 1nF.and i am getting a oscillator frequency 190kHz.

and a same is repeated in one more uc1846, and geeting a oscillator frequency 184kHz.

so what is the tolerance of the IC.

can anyone provide me a solution to get the repeatability from one IC to another.

Thanks

SUDEEP