Is there any literature/more information on C1 and R1 value calculation in the LM134 datasheet, Figure 20: Higher Current Output configuration? I'm planning on using this current source to output 15mA.
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is there any literature/more information on C1 and R1 value calculation in the LM134 datasheet, Figure 20: Higher Current Output configuration? I'm planning on using this current source to output 15mA.
Thanks
Kirby,
Thank you.
Also, will 2 LM134 in parallel work similar to using a transistor to increase the current output?
I have not been able to find additional applications information yet. There is one more source for archives I am still working on that looks promising. I hope to have that info by the end of the week. The part was released over 40 years ago and I haven't seen this question come up recently.