This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC4245A-EP: Unused pins

Part Number: SN74LVC4245A-EP

Do we need unused I/O-pins of Ai and Bi to pull down to GND through resistors?

We could not specify I/O-pin functions of Ai and Bi; because those functions of input or output are depend on direction pin (2-pin) control.

What resistor value is recommended?

Is about 10 k ohm a possible choice?