Other Parts Discussed in Thread: OMAPL138
Tool/software: Code Composer Studio
Hello Ti's technical staff
Thanks in advance for your help.
we have a FPGA + OMAPL138 items,that FPGA(with a Flash using for storage omap'image binnary file)need to boot or update OMAPL138(arm and dsp)via HPI port.
1.I need to confirm that whether OMAPL138 can be loaded success by HPI boot mode?can or can not?
2.i'd like to known how to convert .out file to .bin file in ccs5.5,and on OMAPL138.
3.During the HPI boot of omapl138,how can i change the PLL settings and bringing up the ddr2(setting ddr controller) via hpi port.
4.Do I possibly need two separate boot loaders, one that will just do the initializations normally done in the GEL file or by AISGen and one for the actual code
transfer?
thanks