Other Parts Discussed in Thread: UCC28C45,
I am designing a feedforward control for a simple DCM flyback. Our circuit will operate over a wide temperature range and I am trying to design a temperature compensation circuit. Is it possible for me to get a definition of the temperature dependent voltage drop across the diode between the comp pin and the voltage divider going into the CS pin? I need something pretty accurate like a spice model which accurately accounts for thermal effects. Measured IV data for the diode at -55, 25, and 125 would work for me too then I could build a model of it. Bottom line is I need more information to do my design than is given in the data sheet. I've looked at figure 7 in the data sheet. I think I would be able to deduce the information I am looking for from the plot if the data were collected for any CS voltage other than 0. Maybe that was intentional taking the data at that point to publish? Not sure, but help would be appreciated.