Other Parts Discussed in Thread: SN54AC00-SP, SN54AC02-SP, SN54AC14-SP
Hi,
I'm designing with the TPS7A4501-SP and wish to be able to turn the device output ON & OFF,
Now, the datasheet states a the the minimum ON to OFF threshold is 0.15V (Typical is 0.75V).
I looked at options to deliver the SHDN signal from an FPGA, digital logic and transistor open collector circuits and non of them can guaranty a maximum V_Low<0.15V. the best I could do was 0.3V.
Can you recommend on a driver circuit that will provide such low voltage levels?
Regards,
Itai