This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TVP5150AM1-EP: How to interface and test TVP5150AM1-EP with AM5728

Part Number: TVP5150AM1-EP
Other Parts Discussed in Thread: AM5728

Hello,

I want to interface the TVP5150AM1-EP with my custom AM5728.

Is there any documentary which shows the interfacing of the above mentioned part with the AM5728.

And how to test the part whether it is working or not?

I have read the part page i have the driver after loading the driver how to write the application code is there example code?

Thanks & Regards,

Vijay

  • Hi Vijay,

    As far as I know, once the driver is loaded then the video port should just appear as a valid video/camera source to be accessed through GStreamer, V4L, etc. (depending on the driver used).

    If you can access the I2C bus, then you can read back the status registers to check for things like video lock, etc. This should tell you that the TVP video input and demodulation part are correct.

    Also, I am not aware of any application example code.

    Regards,
    Melissa