Other Parts Discussed in Thread: LM139
Hello,
We have an LM139AWG/883 used to create an edge from a power on reset timer RC circuit and it is failing below 0C, even though the part is supposed to be rated -55 to 125C. The output starts to glitch low a little under 0C and then as it gets colder, the output more resembles a clock.
I see two potential issues in the circuit and wanted to see if these could be contributors or if we could have a bad part.
1) The VCC is 3.3V, which is within the absolute ratings, but not within the 5-30V recommended input voltage.
2) The circuit needs some hysteresis, as seen by some bouncing while transitioning.
Thank you,
Todd