Hi team,
I have a question regarding the SN54S04 Vabs max on the input pin. The datasheet says that the absolute max voltage on the input pin is 5.5V. Does this max rating also apply to transient overshoots? My customer is trying to apply 7V for about 4nS on the pin. Will this degrade the part and cause potential damage?
If the abs max cannot be exceeded, would it be possible to add a Schottky diode between the input pin and Vcc to clamp the transient spike?
Thanks for the help,
Arthur Huang