Other Parts Discussed in Thread: OMAPL138, OMAP-L138
Tool/software: TI C/C++ Compiler
On the basis of OMAPL138 platform, we want to realize 24 way sampling (four independent sampling loops, 4 independent AD, each AD acquisition UA, UB, UC, IA, IB, IC path).
1) chip select EMA_CS[2~5] EMIFA; one for FLASH; and the 4 AD chip, CS to four, missing one; what is the solution?
2) the sampling frequency of 4 AD chips is controlled by PWM; at present, only 2 PWM are known on OMAPL138, and two are missing, and there is a solution
3) there is only one input signal EMA_WAIT for the arbitration, but how does the data ready for the data of the 4 AD chips are close at the same time, and how does the EMIFA handle it? Are there any solutions?