Hello,
I have a board SM320F2808PZMEP which I can't flash with C2000 Series XDS510LC JTAG emulator. I have gone through every connections both on schematic and layout and checked all JTAG pin voltages without success. I have another similar board but with TMS320F2808TZ device that I can successfully flash with C2000 Series XDS510LC JTAG emulator. Knowing that the 2 devices are from the same families, I was wondering if SM320F2808PZMEP which could potentially run up to -55'C might need special settings in the JTAG environment to flash. Basically anytime I would try to flash the board having SM320F2808PZMEP device in the C2000 Series XDS510LC JTAG emulator environment, the section where the image should be chosen is deactivated. I have attached the schematics of the board showing the connections between JTAG connector and the processor for your further considerations. I am using an 8 MHz crystal for the processor.
Regards,