This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAPL137-HT: M size microphone array for beam forming and tracking

Part Number: OMAPL137-HT
Other Parts Discussed in Thread: 66AK2G02, OMAP-L137, 66AK2G12

Hello Experts,

I just have query as

The objective of my work is to develop a M size microphone array (M is from few tens to hundreds) and estimate the direction or arrival for beam forming and tracking. For this purpose i need Hardware and software. The application in indoor acoustics and hence a small anechoic chamber is required. I do want to test it first for few channels only and then to scale up for more channels.

So, i have gone through OMAP L137 with DA830 evm  which gives 8 channel support,Now i want to know that is it possible to implement the above project on same and later on extend it to more channels or do some synchronization of  multiple boards with same configuration.

or else if any other EVM from TI supports multiple Microphone array ,please suggest same.