Other Parts Discussed in Thread: TPS40200EVM-002, PMP7154, , SWITCHERPRO
Hi.
We are happy with the TPS40200EVM-002.
We only need to change the Output - to be fixed at 5V 1A - With all Ceramic output Caps.
(As is used in PMP7154 : Output 5V 1A using only 2x 100μF 6.3V Ceramic output caps.)
Must also change the TPS40200EVM-002's Input Electrolytic Cap - to a Ceramic Cap.
Will use the TPS40200-EP or -HT Chip.
What can we use (or do) to make these few changes?
SwitcherPro™ and WEBENCH® Design Center - might be a to much work - to implement these few changes.
Anybody that can do these few changes?