Hello,
I am considering the use of the LM98640 to connect to a sensor providing several sets of two seperate output lines, one for the REFERENCE level and one for the SIGNAL level. Both signals are presented at the output interface at the same time. Those signals are typically swinging between 1V and 3V.
The datasheet says that the LM98640 is typically used AC coupled but I am afraid that is my case we will lose some information as the REFERENCE signal might not fluctuate much and the SIGNAL might also be slowly changing over a frame. Thus what is left would be a DC coupling of the inputs and the datasheet is giving a CDS mode example in §8.2 but no SH mode example are presented. Am I correct or am I forgetting some essential details here?
My first problem is how to bias correctly if necessary. Figure 17 in §7.3.2 Input Bias and Clamping seems to be indicating that the CLAMP internal signal or the CLPIN extarnal signal will allow to connect the OSx- to the internal VCLP and therefore force a voltage at the OSx- pin. In case of a DC coupling, this means the VCLP voltage will be applied to the sensor output and I doubt it would be a good idea.
Therefore what would be the best solution in term of range and bias?
Regards.