I am seeing an issue with the MSP430F2274-EP at elevated temperatures. Around 65C, the IC gives out of range readings of the A/D converter.
Under lower temperatures, I see the correct values expected from the ADC. However, when the IC is "hot" I am seeing a spurious value for one reading out of say 30 or 40.
Normally, the value out of several channels is ok, but every once in awhile, I see a totally unexpected value. I have looked at the inputs and there is no noise or drop-outs.
I am using a high precision 3.0 volt reference and do not see any noise on the input.
Not sure why, but this is very repeatable on multiple units.
Regards.