Other Parts Discussed in Thread: LM98640CVAL
Hello,
The following information is given in the datasheet:
"CDS Gain = 1x ; OSX = VDD33 (OSX = VSS) ; 384 μA Typ"
"CDS Gain = 2x ; OSX = VDD33 (OSX = VSS) ; -475 μA Typ"
Does that mean that on top of charging the 4pF or 8pF equivalent input capacitance the device connected to both the OSx inputs must be able to source or sink these current for each OSx pin?
Regards.