Hello
Iam using SN54LS193 used in the down converter mode and with input word 1 1 1 1 at A B C B input pin's with clock of 200kHz input.
Could you please suggest how can we calculate the pulse width( time taken to down convert to 0 0 0 0 from 1 1 1 1 input)and for application as the data loaded in the counter it starts down counting with down counting clock signal, at the end of down count it generated a barrow signal which resets the flip flop in the circuit.
Also suggest what will be the input word loaded to generate the pulse width of 8usec and 16usec.
Regards,
RVP