Do you have an IBIS file for this part?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Sean,
I was able to locate another device using the same IO cell. I have modified the ibis model and renamed to only include the BC3350CS model. It uses a model selector, so you need to choose BC3350CS_3P3 for the 3.3V model.
I also used the mean values for a similar package for the RLC of the package. This should be representative.
The component name is XIO2200A.
If this answers your question, please click "Verify it as the answer"
Regards,
Wade