I would like to know if you have stated the failure modes of the component ADC128S102QML-SP? Thanks in advance, Andrés.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I would like to know if you have stated the failure modes of the component ADC128S102QML-SP? Thanks in advance, Andrés.
Hello Andres,
We do not have a listing separate from the datasheet.
Here are the most common issues discussed:
The most important thing is not to exceed the abs max limits. No pins should be taken beyond the abs max voltage shown in the datasheet, even if the current is limited on that pin. If violating abs doesn't immediately damage the part, it may impact the life of the part. We have not characterized the lifetime of the part for operation beyond abs max.
As far as performance goes, none of the imputs should be taken beyond the power supply rails. Taking an unused imput beyond the ralis will impact the reading on the input benig sampled.
The track and hold capacitors are not reset after each sample. The input should be low impedance or residual charge in the parts caps could impact the performance.