I am using the following circuit with UC1903 IC to monitor a negative supply.
R1=11K, R2 = 56K. I am using WADJ = 1V for a +/-10% threshold limit. The IC is powered by +15V which is also potentially divided to 2.5V to monitor using SENSE 1 input. My circuit output is POWER OK pin with a pull up to 5V with a 10K resistor (a LOW indicates voltages monitored are NOT HEALTHY and a HIGH indicated monitored voltages are HEALTHY).
My assumption was, if i float the -Vs input, since there is a 11K across the inverter, Pin 5 will be virtual GND and output of the IC will be "NOT HEALTHY". But i am getting the output still as "HEALTHY". If connect a 5 Meg Ohm resistor from Pin 5 to GND, the output shows "HEALTHY" once in a while and "NOT HEALTHY" other times. Can you help me out with this problem? My circuitry is fixed and i do not have a provision in my layout to connect a resistor from Pin 5 to GND permanently.
1. Is this behaviour expected?
2. How to circumvent this issue and indicate a "NOT HEALTHY" output when i float the -Vs?