This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A4501-SP: Outgassing Test Data

Part Number: TPS7A4501-SP
Other Parts Discussed in Thread: ADS1282-SP, DAC121S101QML-SP, DS96F174MQML, ADC128S102QML-SP, TPS7H1101A-SP, ADC128S102, DS96F173MQML

Hello,

I am requesting information pertaining to outgas testing data on the product part numbers shown below. The data that is of concern is the TML (total mass loss) and CVCM(Collected Volatile Condensable Material).

PN: TPS7A4501-SP

Thanks,

Tyler

  • The engineer responsible for this device is out of the office until Monday. Expect a response then.
    Regards,
    Wade
  • Hi Tyler,

    The TPS7A4501-SP on the TI website is only available as Known Good Die (KGD) or in a hermetic package.    These hermetic packages and KGD do not outgas and testing is not required.  The ink used for marking the package is on the JPL/NASA list as approved for space flight use (no outgassing).

    Let us know if you need additional informtion. 

    -Richard Biddle

  • Thanks for that Information Richard!

    Could you also help determine outgassing data for the part numbers listed below?

    • ADS1282-SP

    • DAC121S101QML-SP

    • DS96F174MQML

    •  ADC128S102QML-SP

    Thanks,

    Tyler Barrett

  • These all fall into the same catagory.
  • Hey Richard,

    I appreciate your fast responses. I have a few more components that I would like to run by you to verify they fall into the same category as the components previously mentioned. The components are listed below.
    • TPS7H1101A-SP
    • LMX2615W-MLS
    • DS96F173
    • ADC128S102

    Thanks,
    Tyler Barrett
  • Hello Tyler,

    TPS7H1101A-SP: Only available as Known Good Die and ceramic/hermetic package - no outgassing concern.

    LMX2615W-MLS: Currently in preview status.  Only available in ceramic/hermetic package - no outgassing concern.

    DS96F173MQML: Only available in ceramic/hermetic package - no outgassing concern.

    The ADC128S102QML-SP is only available as Known Good Die and ceramic/hermetic package - no outgassing concern.

    There is also the ADC128S102CIMT which is a TSOP plastic package. It would require outgas testing which TI does not perform for commercial products.

    Please include the full TI part number on these questions. That would allow differentiation of package types and faster answers.

    -Richard