• Not Answered

AFE4300: continues value

Part Number: AFE4300

HI all,

    I have one question about the AFE4300EVM board. I was using the BCM mode to measure the body impedance. but I just can one value after each time I push the "measure" buttom. How can I get the continues value during a period, like one hour? 

because I want to use the data to determine the human behavior like jump, run, or sit. Thus the individual data means no thing. 

best,

Le

1 Reply

  • Hi Le,

    You can program the AFE for the BCM functionality and capture the output of BCM continuously using "ADC Capture and Analysis" tab.
    Please note that, this kind of capture gives the ADC's data so further computation ( such as calibration, magnitude and phase calculation) should be done offline after saving the data.

    Regards,
    Prabin