Dear, Sir.
AFE44x0SPO2EVM contains 5V, 3V LDO's it on.
TPS7A4901(3V LDO) would be lower output noise because it(low output noise) is the
advantage of TPS7A4901 with putting Cnr/ss it on.
In addition, LC filter(Fc=16kHz) are located following such LOD circuitry.
1. What is the special reason why LC filter put following LDO?
I wonder AFE4490 is so sensitive for the high specific frequency noise?
2. Is there any develpment criteria to be minimized above noise?
Best Regards,