This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Thomas,
There are two analog outputs (with very high voltages) from the TX517.
One is CHA OUTA and the other is CHB OUTB.
We use a transformer to combine OUTA and OUTB together
to create the OUTA-OUTB output to multi-level pulses.
You can see the explanation from our TX517 data sheet and users guide:
also shown below:
For example:
Here is the plot showing:
CHA OUTA (shown in purple color) 5-level
CHB OUTB (shown in green color) 5-level
OUTA-OUTB (shown in Red color) 17-level
(Can be done by using a transformer)
We are using DA2319 Coilcraft transformer which covers freq 50kHz-2MHz range.
Of course if your board design already includes the same purpose like us as using a transformer to do OUTA-OUTB,
then you don't need to use any extra transformer to do so.
Thanks and best regards,
Chen
I do not understand what you mean by "Of course if your board design already includes the same purpose like us as using a transformer to do OUTA-OUTB, then you don't need to use any extra transformer to do so."
What is the benefit of the transformer?
I also wonder what the benefit of Diodes D1 and D2 is in your schematic above. Can I leave those out?
Thanks,
Thomas
Thomas,
The TX517 can be used as a dual-channel, 5-level TX, or a single-channel 17-level TX. To achieve 17-level, you need to use a transformer to subtract OUTB from OUTA. For instance, OUTA=+60V, OUTB=-20V, then XFMR output is then +80V. The diodes are for damping. when the signal drops below ABS(Vdiode), then the output at C11 is isolated from the TX517 and XFMR output.
If this is a multi-channel SONAR type imaging application, please look at our AFE5401 and AFE58JD18, as well.
Thanks,
Chuck
Hi Thomas,
The advantage of using a transformer is:
Each channel output has 5 levels with high voltages.
You can just use one channel output with its own load resistor for that channel.
In this case we don't need to use any transformer.
You can use two channel OUTA and OUTB with different output signals
and connect them to a transformer inputs to generate OUTA-OUTB signal at the end of the transformer output.
In this case the output has 17 levels with very high voltage.
Thanks and best regards,
Chen