Hello,
We have been struggling to use our AFE5809EVM with the TSW1400EVM for a few months now.
The issue is explained in this thread:
In short, the issue is that, whenever we want to capture data from our AFE5809EVM, we get the following error:
I suspect the error is due to the second possible option as shown in the image above, namely, "2. Clock from ADC EVM is not received by TSW Board."
1. I checked the Clock output of AFE5809EVM (P10-58 and P10-66), however, no signal was detected.
2. I checked the JP9 jumper, and I can see the 40Mhz clock frequency which is generated by the Crystal.
Question:
I would like to know why our AFE5809EVM is not generating any clock output on P10-58 and P10-66. So, I would appreciate if someone could share the details of their setup environment with us. What software versions are you using, which windows version and do you use the default board configurations as explained in the user manual?
Thank you so much