Hello,
I am having an issue trying to measure the impedance across my tissue sample. I am trying to send a current through the BCM terminal J36and through my tissue, while recording the voltage it returns in the tissue using the BCM terminal J10. It is working fine when I am making normal tissue measurements. However, when I cut the tissue in half, the circuit appears to be open, and I should be seeing voltage values of 0V, but I am seeing values closer to 1.7V, which is the reference voltage. I am assuming this could be a feedback issue, because the circuit is theoretically open, yet I am seeing a voltage through the tissue.
This is frustrating because I am not seeing what I should be. I might be doing something wrong in the setup, but I cannot find any instructions of how to set this type of circuit up, without using the on board load cell. I am also unsure of which way the alternating current flows through the IOUT terminals. Would a diode ensure it flows one way? The only data sheets and guides are for BCM measurements using external devices like hand-to-hand meters, and that's not what I am doing. I am simply trying to measure the impedance across a tissue via the voltage received, and the output current sent through the tissue.
Thanks for your time!
-Alex