Hello support team,
Our customer is now evaluating the high speed communication of JESD204B using ADS52J90.
I have some questions about the behavior when the following conditions are set.
Data rate of JESD204B = 6.12 Gbps
Frequency of device clock = 102 MHz
L = 4, M = 16, F = 6, K = 4, N = 10, N '= 12, TailBits = 2 bits
Built-in test pattern is used. (No analog input signal is used.)
1. Does ADS52J90 function well when the settings above are set?
(Though it is described as "5-Gbps JESD Interface" in the data sheet.)
2. If ADS52J90 does not function, which part does not work?
(Where is the bottleneck part of ADS52J90?)
Best regards,
M. Tachibana