Part Number: LM98640
Hello,
we intent to use the LM98640 in CDS and Quad Lane Mode at 25 MHz Pixel Rate.
Like described in your data sheet in CDS Mode "the input sampling amplifier has two physical paths (odd/even) through which a particular pixel will be sampled. These two sampling paths are a requirement in the Correlated Double Sampling architecture."
OK - furthermore will be explained that:
"The LM98640QML will indicate (with the TXFRM signal) whether the pixel traveled the even path or the odd path. For all "Odd" pixels, the TXFRM signal is high for three TXCLK periods ..."
But here seems to be the problem - there's ONE TXFRM Signal only but TWO ADC output lanes.
For which of the two output lanes the TXFRM is valid in relation of ODD or EVEN ??? That is not clarified!
Based on this feature we got In front of the design procedure from our customer following questions (experience from another project):