In AFE4300 datasheet section 8.1.2 Handling Oscillation of the Excitation Amplifier. I see a recommendation to use series Rcm, Ccm (1K, 1nF) on one of the RPx pins to prevent oscillations. However this will also have the calibration resistor connected between RPx & RNx. Wont this affect the calibration slope & offset value ?
Suppose i have a 1 Kohm between RP1 & RN1 for calibration and also Rcm series Ccm on RP1 pin what should be the resistance value i should use in the software for the slope formula ? Eq 1 sbaa202
thx
sundar