• Resolved

ADC32RF82EVM: Device Communication Error: FT_DEVICE_NOT_FOUND

Part Number: ADC32RF82EVM

Hi,

We currently try to use the ADC32RF82EVM board in combination with the TSW14J56 board. The communication to TSW via HSDC Pro is working.

But we cannot setup the communication to the ADC board. We followed the instructions from the user manual and also the "FTDI Driver Installation Procedure.pdf". We also tried from two different PCs.

There is always this error:

Device communication error: "FT_DEVICE_NOT_FOUND"

Software Version of the GUI (ADC32RFxx EVM GUI)  is: 4.1

I choose this device in the selection box: ADC32RFxx

The voltages on the testpoints of the board are matching the schematics. 

Thanks a lot in advance for your support!

Tobias