This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL5500 LNA

Other Parts Discussed in Thread: TL5500

Hi,

Can we design LNA to meet below specifications using TL5500

RF CHARACTERISTICS:

OPERATING FREQUENCY

63.87MHz

OPERATING BW

1MHz

GAIN (S21)

28dB

NOISE FIGURE

0.4dB

INPUT IMPEDANCE REAL

1 Ohm

INPUT IMPEDANCE IMAG

-3 to 3 Ohm

OUTPUT RETURN LOSS (S22)

-20dB

REVERSE ISOLATION (S12)

-70dB

Output intercept point first order (OIP1)

5dBm

Output intercept point Third order (OIP3)

15dBm

STABILITY K

1

SATURATE RECOVER TIME

8uS

ESD AIR CONTACT

16kV

ESD DIRECT CONTACT

6kV

DC OPERATING PARAMETERS :

VOLTAGE

10V

Current

19mA

Temperature

15 to 50 C

ABSOLUTE MAXIMUM RATINGS :

Maximum power input

30dBm

Voltage

12V

Thanks,

Ravikiran S