• Resolved

ISO5852S: Vcc2 Under Recommended Operating

Part Number: ISO5852S

Team-

My customer is interested in using the ISO5852 to drive a FET with a +10V Gate drive. The ISO5852 has a recommended minimum of +15V but has ABS minimum at -.3V. What would be the implications of running Vcc2 at 10V or 12V to support their application? Would that mode of operation work or would there be significant performance differences?


Thanks,

Alec