• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Applications » Motor Drivers » Motor Drivers Forum » DRV8301 faulting immediately on start-up
Share
Motor Drivers
  • Forum
  • Announcements
  • E2E Wiki
Options
  • Subscribe via RSS

DRV8301 faulting immediately on start-up

DRV8301 faulting immediately on start-up

This question is not answered
Joe Hlebasko
Posted by Joe Hlebasko
on Dec 03 2011 10:10 AM
Prodigy30 points

I am experimenting with the DVR8301-HC2 kit.  I was able to work my through the basic GUI and then the Build steps with the code getting my motor to spin at the right steps. I started to add some code to the existing BLDC_Int project to read the potentiometer to set the speed.   I started getting a driver fault as soon as I enable the motor.  All the fault bits report "1". I've gone back to the stock code and I get the same result. I've done numerous power cycles to the same effect.  So it looks like I did something to the DRV8301 driver.  I am kind of baffled by all of the faults being set, unless this just means the driver chip has been damaged.  Where should I start looking to confirm what happened?

DRV8301
Report Abuse
  • Reply
You have posted to a forum that requires a moderator to approve posts before they are publicly available.
All Replies
  • Ryan Kehr
    Posted by Ryan Kehr
    on Dec 05 2011 17:42 PM
    Genius13845 points

    Joe,

     

    If you go back to the original code that shipped with the EVM and GUI, do you have the FAULT problem?  If so, I would say the chip might be damaged.  

     

    What is the revision of your board?  We originally distributed some REVB versions of the board that were sensitive to GND noise on the DVDD and AVDD decoupling and FAULTs would occur.  We add "blue wire" fixes on the board.  If you have a REVC version, the PCB was fixed to address this.  

     

    Finally, please check that you have a delay between ENABLING the DRV8301 with EN_GATE and sending PWM commands.  This is specified in the datasheet as 10ms.  If you do not wait this amount of time, faults can occur.  

     

     

    Ryan Kehr

    Motor Drive Application Manager

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Joe Hlebasko
    Posted by Joe Hlebasko
    on Dec 06 2011 00:12 AM
    Prodigy30 points

    Ryan,

    Thanks for the response. I went back to the original code and have the fault occurring,  I check the revision of the board it appears to be a rev C board per the silkscreen on the top of the board.

    I verified that the the stock delay is still present.  currently the delay is 10ms.  I even increased the delay to no effect. The fault LED starts to light as soon as the EN_GATE signal is brought high.  I added some breakpoints and found the following:

    • The fault LED lights as soon as teh EN_GATE signal is brought high
    • checking the return value from the two SPI write calls indicate a fault condition of a overcurrent on FET High-B and FET High-A
    • checking the return value after writing cntrl_reg2, indicates an overcurrent on FET high-A
    • If I let the code run, and force reading of the two stat registers, I see the fault bit set, without any of the other fault bits set in either of the stat registers
    • Sometimes I see the fault bit set, but the status registes do not contain a set fault bit.

    This last set of tests I did not have a motor connected and was doing the build level 1.  I don't understand why/how I am seeing overcurrent faults without a motor attached.

    Any other ideas to look at?

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Ryan Kehr
    Posted by Ryan Kehr
    on Dec 06 2011 11:18 AM
    Genius13845 points

    Joe,

     

    In control register 1 (address 0x02), what is your setting for bits D6-D10?  This sets your OC level per table 9 in the datasheet.  

     

    Also, we can completely rule out some "false" OC reporting by disabling this protection.  Write D4-D5 = 1 in Control Register 1 (Address 0x02) to disable OC sensing and reporting.  If you are still getting a fault, then we need to look somewhere else.

     

     

    Ryan Kehr

    Motor Drive Application Manager

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Joe Hlebasko
    Posted by Joe Hlebasko
    on Dec 06 2011 18:53 PM
    Prodigy30 points

    Ryan,

    The OC limit is switch Vds=.358V (which was the default setting from the original code).  I disabled the OC protection.  The fault LED flickers the I am unalbe to get the motor to spin.  The status registers both read all ones.

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Ryan Kehr
    Posted by Ryan Kehr
    on Dec 07 2011 17:25 PM
    Genius13845 points

    Joe,

     

    At this point, I would like to try a new IC on the board.  Do you have the tools to replace the IC?  You can order some free samples from our website.  

     

    Ryan Kehr

    Motor Drive Application Manager

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Kelly Meemken
    Posted by Kelly Meemken
    on May 14 2012 11:17 AM
    Intellectual435 points

    How do you view the faults on the drv8301.  Is there an area in the GUI that specifies which problem triggered the fault?

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • ChrisClearman
    Posted by ChrisClearman
    on May 14 2012 14:32 PM
    Mastermind23195 points

    use the watch window with real-time mode on

    DRV8301_stat_reg1.all
    DRV8301_stat_reg2.all

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Kelly Meemken
    Posted by Kelly Meemken
    on May 14 2012 14:58 PM
    Intellectual435 points

    I'm trying to run through the 7 steps using the PM sensorless project for FOC control.  My program continues to get caught in a while loop (located below) and I don't see how it will ever get out.  How do I set EnableFlag to TRUE?  Do you use the GUI when running from RAM or is that only when running in FLASH.  is there a FOC program that I can load into flash for the drv8301?  Is there any better documentation for running the PM Senserless program (FOC) than "DRV830x-HC-C2_kit" How to Run Guide? 

    // Call Flash Initialization to setup flash waitstates

    // This function must reside in RAM

    InitFlash();

    // Call the flash wrapper init function

    #endif

    //(FLASH)

    // Waiting for enable flag set

    while (EnableFlag==FALSE)

    {

    BackTicker++;

    }

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • ChrisClearman
    Posted by ChrisClearman
    on May 14 2012 15:12 PM
    Mastermind23195 points

    read

    C:\ti\controlSUITE\development_kits\DRV830x-HC-C2-KIT_v104\PM_Sensorless\~Doc\Sensorless FOC of PMSM.pdf

    I think your world will get more clear....

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Kelly Meemken
    Posted by Kelly Meemken
    on May 15 2012 10:18 AM
    Intellectual435 points

    That helps a lot but after building level 1, I disable the realtime option, rebuild the project (level 2 which automaticle updates the program on the chip because I didn't disconect), reset the CPU, reset the program and then re-enable the realtime option and the real time doesn't seem to work.  Am I missing a step in there?  The weird thing is when I go to disable the realtime option, the watch window appears to update although it says "could not read memory location" next to every variable but I can see the window updating.  I had this problem yesterday and I completely restarted my project over and deleted my workspace and it seemed to fix it for level 1 but when I try to move to level 2, it acts up again.

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Kelly Meemken
    Posted by Kelly Meemken
    on May 15 2012 11:46 AM
    Intellectual435 points

    I fixed the problem above by connecting to the target and loading the .out file separetly.  At level 1, I am not seeing the signals output on channel A, B , and C like I should to verify that the signal is indeed outputing before connecting the motor in level 2.  Any thoughts?

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use