I would like to see an application circuit for the DRV595 TEC driver IC.
After reading the datasheet, I don't understand how it is used. The datasheet states states "The typical circuit used for this application is to have two feedback loops one for constant current, and the second to monitor the temperature, and provide adjustments to keep a constant temperature on the laser diode. An error amplifier is used to combine the two feedback loops, along with a control signal from the system. The output of the error amplifier is then fed into the DRV595.
Fundamental question: How do you sense the current for input to the constant current loop?
-Bob McKnight