I am using the 8301-RM48 motor kit.
When I run Project "RM48L952_foc_encoder_speed" for speed control of the motor.
When I set the reference speed to be "0.05", which is "172rpm", the motor is still running properly.
But if the reference speed is set to be "0.04", which is "138rpm", the motor just stops.
Is there anything I can do to make the motor run at a low speed, say "10-20 rpm"?