Errors in LAB 5c.
From lab05b to lab05c, we switch from FOC to MOTION. Did that
We populate the new user.h file with values used in from the user.h file in FOC. Did That
in LAB05b use we opened a c file called proj_lab05b.c and built our project. I noticed that LAB05c has no such file.
The errors I get are:
Description Resource Path Location Type
<a href="file:/C:/ti/ccsv5/tools/compiler/dmed/HTML/10234.html">#10234-D</a> unresolved symbols remain proj_lab05c C/C++ Problem
unresolved symbol _main, first referenced in C:/ti/ccsv5/tools/compiler/c2000_6.2.0/lib/rts2800_ml.lib<args_main.obj> proj_lab05c C/C++ Problem
#10010 errors encountered during linking; "proj_lab05c.out" not built proj_lab05c C/C++ Problem
In addition to the USER_MOTOR settings, it is important that you copy ANY field that you modified as part of the previous labs or as part of your hardware design process into this new user.h file. Did That
I have removed and installed the project files several times, checked to make sure I was in MotorWare and in the right directory, don't know what the problem is. I could build the other projects just fine.
Can any one suggest what it might be that I need to do, or what the problem might be.
Thanks,
David