Hi for everyone,
This is the first time that i use the TI forum. After many searching, there are some questions didn't answered in my head. Please help me.
I'm using the DRV8332 to drive a BLDC blower. This motor has a peak of power on 192W (32V/6Amps). On my application, I'm using a PWM frequency of 72Khz, my bootstrap capacitor value is 100nF (indicated by the datasheet) and my OC_ADJ resistor is 22Kohm. If necessary, i can put here the detail schematic here.
So, my questions are:
- What is the better voltage rating of the bootstrap capacitor?
- At 72Khz, the value of 100nF (bootstrap capacitor) is the better choice?
- On all of the PVDD_x pins, i'm using an 100nF ceramic cap with 50V of voltage rating, Is this the better choice? I mean, what is the better voltage rating for a cap on the PVDD pins?
An early answer will be appreciated,
Best Regards,
Anderson.