We have built a new 2-phase motor and are having problems using the DRV8711EVM board to control the motor. We're getting very narrow 5us pulses with a duty cycle of 18% (37kHz) out of the DRV8711EVM board. Of course, it's likely that we have a problem with the new motor, but nonetheless the DRV8711EVM pulses seem too narrow.
The DRV8711EVM works fine with the stepper motor that came with the kit and the pulses looked like those shown in the slva632.pdf doc when driving that motor.
Any ideas on what could be causing the narrow pulses?
Thanks, John