Hi,
I have gone through the power dissipation calculation for my 8825 application.
Application specs:
Stepper Motor: 5.7 ohms per coil, 1A max per coil.
multistep set to 1/4
Very low frequency needed for step function (1/4 turn within 1 second, then stopped until needed again at random intervals).
Input Va and Vb power supply: 15Vdc
For the power dissipation calculation, I assumed slow decay, and the Switching frequency very high compared with true to provide some buffer. My current limiter (Vref) is set to limit at approximately at 0.95A, though I used 1A for ease of calculation.
The total I came up with is 1.4W. At this power, I am very safe for temp issues even at our highest expected ambient, so I have no issues there. What I need to know, however, is what is the current draw on my 15Vdc source at each Voltage (a & b) input? I need this so I can request the proper trace width(s) to the PCB designer.
Is it as simple as I(input) = P(total) / V(input) ----> I = 1.4W / 15Vdc = 0.1A ? Or are there other factors to consider before we can get from total power dissipation to input current draw at the source voltage pins?
Thank you,
Matt