I'm creating the footprint for the DRV8801PWP in Orcad PCB Editor and could use some help. Hopefully some of the gurus on here use Orcad and PCB Editor!
I'm using Pad Designer to create the pad for a 2 layer board. I'd like the thermal pad to be part of the ground plane. Here is a list of my padstack layers:
Begin Layer Rect 5.00x3.4 (in mm)
Default Internal: Null
End Layer: Rect 5.0x3.4
SolderMask_Top: Square 3.00
SolderMask_Bottom: Null (I don't want a any of the pad on the bottom exposed)
PasteMask_Top: I haven't figured out what this should be yet
Do I have this right?
I also have specified multiple drill in a 2 rows by 2 columns pattern to get the thermal vias. The Drill diameter is 0.33mm per the spec.