Hello,
Customer wants to know startup time of boost converter from B_EN changes to High.
I have already answer answered as follows.
“The time until the boost reaches it's final value is strongly depending on the input voltage, the coil, the boost capacitance, the load, the resistor on GNDLS_B and probably some other parameters. Best would be to read out the boost under voltage flag of STAT1 resistor and wait until it goes low.”
Please answer following additional questions related above requirement.
Q1: startup time of typical application
Please advise minimum and maximum startup time in case of “Figure 16. DRV3201-Q1 Typical Application Diagram” of datasheet (L=22uH, C=1uF, GNDLS_B resistor=330m ohm).
Customer wants to know how the startup time varies.
Q2: V BOOSTUV threshold
Please advise if V BOOSTUV threshold (11V min, 11.9V max) is same in both case of BOOST voltage is increasing and decreasing, or different.
Does it have Hysteresis?
Q3:
In case of V BOOSTUV doesn’t have Hysteresis, are there any risk that boost under voltage flag is unstable near the threshold voltgage?
Best Regards.