Hi,
Am using DRV8313EVM in stand alone mode.It is working fine in normal condition but during power ON/OFF continuously some time it is getting stuck up.when i press the manual reset button/when the supply removed and given again it is working properly.
kindly give any suggestion for this problem.Controller is MSP430G2553.Below are my initial system variables in config.c,speed control is with duty cycle
INTEGRATION_CONSTANT = 2000;
START_UP_DUTY = 1; //%
START_UP_MAX_DUTY = 30; //%
INCREMENTAL_DUTY = 1; //%
INCREMENTAL_TIME = 4; //mS
WAIT_TIME = 48; //mS
SPEED_DUTY_MAX = 97; //%
SPEED_DUTY_MIN = 10; //%
SPEED_RAMP_CYCLES = 2;
Hysteritic_Control = 2;
State = 1;
Speed_Control = 1;
Rotation = 0;
Thank you in advance