We have some boards ( news) that one of the drv8432 are no working . I would like to know where is our mistake.
We use 4 per board , two are working and two drv8432 are not working.
Symptoms in one boards
VDD=12 V, PVDD = 24V, M1=M2=M3=GND, ADJ = 100K to AGND
I would like to ask what can be the problem that FAULT goes low; OTW = (hight) and all output are set to . The motor is working properly, and not short in any point is found .
The motor is not moving , seems that drv8432 detects a short in some place, where can be .
OUTA=OUTB=OUTC=OUTC=11V , and the controller is generating PWM signal , VCC1=5 V , VCC2 =3.3 V ara both OK , current consumption normal, (same when the boards is working properly )
Regards
Albert
What can be the problem