I want to control an AC Servo Motor APM-SC05ADK-9 with the Motordriver DRV8302.
For that, I use as basic program the PM Sensorless example and change the code for my usage. The program works and the motor is moving.
But, if the torque is to high, or even the speed, the motor stop and I have to restart my debug session. I looked into the control and status register, to identify the problem, but I could not find anything.
I appriciated any help and assumptions to identify the error.
Jan