This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Will the DRW8312 operate with the logic voltage at 12 VDC and the motor voltage between 9 and 14 VDC?

Will the DRW8312 function if the motor power voltage is below the logic voltage?  I would like to use the DRW8312 for quadcopter bldc motors.  I can provide regulated 12 VDC for the logic but the motor power voltage will vary from approx. 14 to 9 VDC.